AXIS#.EIP.QUICKSTOPACTION

Description

The AXIS#.EIP.QUICKSTOPACTION parameter allows an axis' quick stop action to be modified and configured when commanded via the CIP Sync Command Assembly.

Note: If this parameter is written with a quick stop ongoing, the new setting will only apply to the next quick stop. The ongoing quick stop will still use the option that was selected when the quick stop was started.

Context

For more information regarding the usage of quick stop in CIP Sync, see CIP Sync Command Assembly Data Structure (105).

Usage

Value

Description

Behavior

1

Use_Profile_Dec_And_Disable

Performs a stop using profile deceleration ramp (AXIS#.FBUS.DEC) and transitions into the Switch On Disabled state; axis will disable.

2
(Default)

Use_CS_Dec_And_Disable

Performs a stop using AXIS#.CS.DEC  deceleration ramp and transition into the Switch On Disabled state; axis will disable.

5

Use_Profile_Dec_And_Stay_Enabled

Performs a stop using profile deceleration ramp (AXIS#.FBUS.DEC) and stays in Quick Stop Active; axis will stay enabled.

6

Use_CS_Dec_And_Stay_Enabled

Perform a stop using AXIS#.CS.DEC deceleration ramp and stay in Quick Stop Active, axis will stay enabled.

Versions

Action Version Notes
Implemented 02-11-03-000

General Information

Type

Read/Write

Units

N/A

Range

[1, 2, 5, 6]

Default Value

2

Data Type

Integer

Stored in Non-Volatile Memory

Yes

Variants Supported

EtherNet/IP drives: AKD2G-SPI

Industrial Ethernet Information

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

7554

1

7554 (0x1d82)

AXIS1.EIP.QUICKSTOPACTION

Signed16

Read/Write

Yes

73090

2

7554 (0x1d82)

AXIS2.EIP.QUICKSTOPACTION

Signed16

Read/Write

Yes